This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF86EVM: can work with TSW14J56EVM/TSW14J57EVM?

Part Number: DAC38RF86EVM

The DAC38RF86 evaluation module (EVM)  is designed to work with the TSW14J56EVM (Rev B and up).  1. What does  (Rev B and up) mean for? 2. Can DAC38RF86EVM work together with TSW14J57EVM ?

  • User,

    The TSW14J56EVM Rev B is an older version of the board which used a USB 2.0 interface. TI is no longer providing support for this version. The latest board available is the TSW14J56EVM Rev D, which has a USB 3.0 interface. The TSW14J57EVM rev E board, which has a FMC+ connector, is designed for boards using the  JESD204C standard. This board is also backward compatible with JESD204B boards using the standard FMC connector, such as the DAC38RF86EVM.

    Regards,

    Jim