This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM15851: Driving LM15851 diff SYNC~ input with an LVDS driver

Part Number: LM15851

Hi!

As I've seen in LM15851EVM, SYNC~ input of the LM15851 is directly driven by TSW14J56's FPGA diff output. Is that output is configured as an LVDS output?

If so, it doesn't meet common mode voltage requirements for the LM15851 SYNC~ input specified in the datasheet, as LVDS driver has common mode voltage around 1.2V and required range is 0.64V to 1.1V (Recommended Operating Conditions table, p.10).

Have I missed something? Can you give some comments?

Best regards, Vic.