Other Parts Discussed in Thread: PGA280, ADS131E08, OPA192
Hi,
I'm considering using an 8 channel ADC such as the ADS8598H (+-10V). I also like the functionality (a good number of gains) offered by the PGA280 along with its robust input protection features. My requirements is for a multi-range input from +-10mV to +-10V.
However, in order to pair the two (yes, I know I will need a PGA280 for each channel), I will have to convert the unipolar output (0V-5V) of the PGA280 back to a bipolar +-5V (10V range) with another op amp.
Is this a good approach or is there a better way to achieve my requirements?
Thanks,
Steve