This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400EVM: DAC3171EVM custom application using Quartus II

Part Number: TSW1400EVM

Hello!

First of all, apologies for my bad English I hope you can understand my question :).

I have a TSW1400EVM and a DAC3171EVM. I have been working with the two boards using HSDC pro and the DAC3174 applications. I am also been able to create a custom program in VHDL in quartus II (turning on some LEDS or a counter with the local oscillator of the board), and loaded to the board using HSDC pro successfully.

But now, I would like to make a custom program to control both boards (TSW1400 and DAC3171EVM). For example, I would like to create a CLK signal from CDCE62005 (from a given CLK in the J9 connector),use this signal as a main clock of my application and then send data back to the DAC. Is it possible to do something similar to this? If so, could be possible to get some kind of code (doesn't matter if it's verily or vhdl) to see how works the iteration of both boards?

Thank you for your assistance.

Best regards,

Ignacio