Other Parts Discussed in Thread: ADS8678
Hello E2E,
I Looking for EVM of ADS8674, I could not find it.
Is it possible to evaluate ADS8674 on the ADS8678 EVM by implementing ADS8674?
Is GUI saported for ADS8674?
Regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Cynthia,
> the softwre should also be able to support the devices
Does GUI is able to control for ADS8674 on EVM in default? or need to revise?
And,
Is simple-capture-card include with the ADS8678EVM at shipout?
Regards,
ACGUY
Yes, the EVM PDK will come with everything you need to get it up and running. And the software to support the EVM and the devices is available on the EVM PDK website as well as in the Tools and Software tab for the ADS8674
You could download the softwarebefore hand, you do not need to order an EVM to be able to download the GUI, so you can familiarize yourself with it as well
Regards
Cynthia