This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5474: ADS5474 application, TSW1200 verilog source code request

Part Number: ADS5474

Hi Richard P. , or anyone who may be able to help;

I am planning to use ADS5474 in one of my applications, and the availability of  supporting verilog code like the one in TWS1200EVM would be a tremendous  help to me, and would be very much appreciated.  Email: hengjie844@gmail.com

Thanks.

H.M.

  • Hendrick,

    Richard P has retired. Your best bet is download the ADC firmware under the TSW1400EVM product folder on the TI website. TI no longer supports the TSW1200EVM.

    Regards,

    Jim

  • Hi Jim, Thanks for the reply. I am aware of TSW1400EVM, and it is Altera based. The reason I am requesting the source code of TSW1200 because my application is Xilinx FPGA based, and thus it would be easier to port TSW1200EVM verilog code as it would use Xilinx macros. Any chance I can have TWS1200EVM verilog ? I don't care if the board is already obsolete, as I am using my own Xilinx board. Thanks again.
    H.M.