This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1675: which drive circuit for clock buffer?

Part Number: ADS1675
Other Parts Discussed in Thread: SN74AHC1G32, SN74LV1T32

Hi,

which is the recommended drive circuit from the 3.3V clock source to the 5V CMOS input of the ADS1675 while fulfilling the specs? Jitter must be low.

Thanks
Fred