Hi,
I have a TSW14J10EVM-CB high-speed data converter board for zc706 and ADS54J66 board.
Where can I find Xilinx Vivado project for use the HSDC Pro software package?
Thanks,
Kiman
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kiman,
Follow the instructions in the attached file. This example source code is script based. It supports ZC706, VC707, and KC705, depending on what parameters are selected in the script file.
Regards,
Jim
Hi Kiman
Here is a file that should enable that mode. However since I don't have that hardware combination I haven't verified it.
Copy this file to the folder location below:
C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\14J10ZC706 Details\ADC files
When you start up HSDC Pro and connect to the TSW14J10EVM you should now see the needed ADC/mode. Let us know if you have any issues getting it to work.
Best regards,
Jim B
Hi Jim,
I tried test with a new configuration file, but found DDR read timeout error.
Board detection is fine, and I can see ADS54J66_LMF4421
AD54J66 board configuration file:
LMK_Config_LMF_4421_491p52_MSPS.cfg
ADS58J63_burst_mode_8_bypass.cfg
ADC board DC supply voltage is 5V, current is 1.343A
zc706 FPGA board LED L,C,R is blinking after bitstream file loading.
7510.ZC706 ADS54J66 4421 Setup.pptx4188.ADS54J66_LMF_4421.iniKiman,
Please follow the start up guide attached and let me know that you can get a valid capture with this setup. I just tested this with our hardware with no problems.
Regards,
Jim
Kiman,
I think the issue is with the clocks going to the FPGA. The Xilinx firmware requires two clocks. Please take a look at the TSW14J10EVM User's Guide for more information regarding these two clocks and how to them to the correct frequency..
Regards,
Jim
Kiman,
Go the ADC GUI and click on the LMK0428 Clock Output tab. Set the DCLK divider to 6 for CLKout 0 and 1 and set the divider to 12 for CLKout 12 and 13. In this mode, the FPGA needs a reference clock of 500MHz, so this clock divider should be the same frequency as the ADC clock divider and the core clk divider should be 2x of this (12). In HSDC Pro, the ADC output rate will be 500MHz.
Regards,
Jim
Hi Jim,
Some reason, my zc706 board and AD54J66 reference design doesn't work properly with HSDC Pro.
Good progress is yesterday I did readout 250MHz with several configuration mode but 500 Mhz mode-8 is not working.
If you can work with your setup please send your all configuration file.
Thank you for your support and have a good weekend.