This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: ADS1298

Part Number: ADS1298

hi,

   Using the ADS1298R to achieve respiratory function, encountered the following questions:
1. We are currently mainly confused: Schematics R24 and R27 are not attached at present. Use IN1P/IN1N as the respiratory wave acquisition channel and the data is normal. At the same time, it will affect other ECG data acquisition (IN2~IN8). The chest lead V1 is not collected. ;
       Will the respiratory wave and ECG acquisition be performed at the same time? What is the method of implementation?


2. Please help review the attachment. Is there a problem with the schematic design?

ADS1298R.pdf

3, the current register configuration: