Other Parts Discussed in Thread: ADS805
Hello,
I have a project that I get adc1175-20 mhz measured continuously a specific signal. If voltage max value is in about RT-RB, for example 4,30 volts, suddenly digital ports begin to show 0.30 volt or may be more or sometimes I read on digital outputs 30 it means 0.58 volt and it suspends that level. As if chip has max reference voltage is 4.30 volts and when Vin exceeds that limit, digital outputs show rest of what is left from 4.30. It is like mod operation in math. Or dividing operation in math. I have measured several times Vrt-rb and I am pretty sure that it was 5.00 volts or sometimes little bit more it has been changing -+0.01 volt.
All coupling caps like what is mentioned in datasheet and Vin gets driven by 10 mhz operational amp with voltage follower mode.
Vrt connects directly 5 volts Vrb connects directly to ground.
What would be the problem?
Thank you
Regards