Part Number: ADC32RF80
Other Parts Discussed in Thread: ADC32RF45
Hello
The ADC32RF80 is a dual channel device. There is a single ADC sample clock input.
a) Is there any way to introduce a phase offset in the ADC sample clock to the second ADC input channel relative to the first ADC input channel?
b) I have included a block diagram from the ADC32RF80 datasheet (SBAS774A MAY 2016, REVISED DECEMBER 2016) below:
This block diagram shows a "0/180 Clock" block to the second input channel (INBP/INM). Can this block be used to introduce a 180 degree offset in the ADC sample clock for the second input channel? If so, how is this 180 degree offset enabled?
c) I can't find a similar block in the ADC32RF45 datasheet. Does the ADC32RF45 include this functionality as well?
Thank you.
Gavin