Hello,
I am wanting to interface the DAC8560 to my laptop via USB. I was thinking of using some sort of USB to SPI adapter like this one: http://www.ftdichip.com/Support/Documents/DataSheets/ICs/DS_FT232H.pdf.
I am having trouble figuring out how to interface the /SYNC pin on the DAC8560 to the FT232H. I understand that SCLK is SCK and DIN is MOSI, but what would /SYNC be for the standard SPI wiring (MISO, MOSI, SCK, /SS)? Would /SYNC just be /SS? I may also want to add a second channel in the future and I can see I can do that with the EVM, so I am looking for something that would accommodate this requirement as well.
Thanks,
Sheldon