Part Number: ADC12D1800RFRB
Dear All,
I need to be able to digitise an RF signal at a minimum of 1 GS/s, process the samples (in an FPGA or CPU), and stream the result to a computer at a rate of at least 1 Gb/s.
Is it possible to achieve a transfer rate of 1 Gb/s to a computer with this board?
I notice that the board has a USB 2.0 interface only, which presumably would mean the maximum transfer rate would be 0.48 Gb/s.
Would it be possible to modify this board with a USB 3.0 interface instead? Or another high-rate interface?
Is there an alternative board that can achieve a transfer rate of 1 Gb/s to a computer?
Hope somebody can help.
Matthew