This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1131: Setting up communication via ADS1131 and Arduino

Part Number: ADS1131
Other Parts Discussed in Thread: ADS1230, ADS1118, ADS1120

I have soldered the IC and connected it as given in the data sheet ; but instead of weightstone bridge, i have coonected a battery (so as to obtain the adc value of battery).

My question is, on starting the SPI communication, can we get the ADC value read on arduino? And there is no Slave Select (SS) pin; So as to start communication via SPI.

Or there are any other connections? as I see evaluation board (ADS1131-REF)also available for the same.