Hi,
We're not sure about the definition of 20% Resistance Tolerance mentioned in the datasheet.
As I know, this chip offer end-to-end resistance as 100 kΩ with 256 steps.--> The step size is 100kΩ/256.
Considered the case of the 128th step, the value should be 50kΩ. Which description as below is correct about the 20% Resistance Tolerance?
- The resistance value could be in the range from 50kΩ x 80% to 50kΩ x 120%
- The resistance value could be in the range from 50kΩ-100kΩ/256 x 20% to 50kΩ+100kΩ/256 x 20%
Thanks!
Antony