Hi,
For the AMC1203, I have another questions. can you kindly help me answer these questions?
1. When the input voltage is zero, then what's the period of MOUT?
2. And what is the corresponding period when the input voltage is extended to +280mV and -280mV?
3. The period of MOUT is constant or variable?
4. what's the relationship between input voltage and MOUT duty cycle?
Thanks & best regards.