Hi support team,
On page 60 of the data sheet there is a description of Section 10.1 "Power-Supply Sequencing".
According to it, If AVDD ramps before DVDD, then the low-side switch is in an unknown state and can short the AIN3/REFN1 input to AVSS until DVDD has ramped.
[Question]
- If AVDD ramps before DVDD, will AIN / REFN 1 and AVSS be always short-circuited?
- Is this short circuit always solved when DVDD comes up?
Or is there any case not to be solved??
- If the above short circuit can be tolerated, may AVDD be ramped up before DVDD?
- Regardless of the order of power-up, if only the communication is started 50 μs after stabilization of all the power supply, does no problem occur at all?
Sincerely,
M. Tachibana