This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5444EVM-CVAL: Package clarification

Part Number: ADS5444EVM-CVAL
Other Parts Discussed in Thread: ADS5444, ADS5444-SP

This eval board is listed for the ADS5444-SP, but the user guide lists the specifications for the ADS5444 commercial version.  Can someone clarify which chip is included with the eval board?

  • Hi,

    The ADS5444EVM-CVAL contains the ceramic space grade /EM unit on it and not the commercial grade device. The software GUI used to control these two devices is the same so the commercial GUI has been reused to support the space grade device.
    Thanks
    Christian