Hello guys,
One of my customers is evaluating ADS8326 for their next products. They found very strange phenomenon in the evaluation. The phenomenon that any data between 16242(3F72h)~16383(3FFFh) are not output from DOUT regardless the input voltage ("+IN" voltage - "-IN" voltage) as the attached graph. Also any data between 49024(BF80h)~53247(CFFFh) are not output but the graph is not attached.
They are using the circuit same as Figure 44 on page 27 in the device datasheet(SBAS343C). Also their evaluation conditions are that "-IN" terminal voltage is 0V^0.5V, "+IN" terminal voltage is less than "REF" voltage +"-IN" voltage, "REF" voltage is about 4.0V and VDD is 5V.
Do you know any cause of this phenomenon? If you know, could you give me your reply?
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.