Hi Team,
Regarding the ADC12DJ2700 device:
1. Datasheet p.11, VID (Input voltage, peak-to-peak differential), for CLK+/-, SYSREF+/-, units of VPP-DIFF:
See enclosed pictures (from the LMK datasheet):
Does VPP-DIFF refer to VID or 2*VID ?
2. Same as (1) for INA+/- on p. 11 (units of VPP-DIFF) and VIN_FSR on p.12 (units mVpp).
Both Seem to describe the same value but with different units.
Does it refer to VID or 2*VID ?
3. SCLK, SDI, SDO, SCS are limited by VA19 (table on p. 10).
However, SCS on pin description p. 6, has a 82K PU to VD11.
Please advise.
4. What is the tolerance for ZT of 110ohm (datasheet p.13)?
Thanks,
Shlomi