This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J82: Is there an example of DAC38J82?

Part Number: DAC38J82


Are there any examples of configuration registers?

I use ALTERA FPGA 

LMFS :4211   DAC_CLK:400m 

I use the register value generated by GUI and configure DAC through SPI, but I can not output the desired waveform all the time.

Do you have a good example?