This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7263: maximum clock frequency

Part Number: ADS7263

Hi,

We are developing an application with two off ADS7263 running them in half-clock mode at 20MHz. The tolerance on the clock source is 1%, so some ADCs could see a clock frequency of 20.2MHz. Clearly this exceeds the maximum in the data sheet. Can you say whether this presents a real problem? If so then how would the performance of the ADC be affected? (Any design change to reduce the clock frequency would be problematic for the stage of development of the application.)

Best Regards

Richard