This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1305M05: Sinc3_16 and ripple wave relation ship

Part Number: AMC1305M05

Dear E2E:

  I Use AMC1305M05  as a sense currents  in green energy system. 
  
  In no load conditon:  sample rate: sinc3-16  the  ripple wave about channel 1 was a little high, but the channel 2 is normal;

But i change the sample rate: sinc3-32  the  ripple  wave reduce quickly  and the channel 2 still is normal;

  i have double check the GND & VDD net is fine, the schematic are the same. so i was little confused what's the reason?
  i also do load condition , the situation is same.  
             sinc3-16:  channel 1 is bad; channel 2 is fine;
             sinc3-32:  channel 1 is fine; channel 2 is fine;

schematic: