Part Number: ADS1220EVM
Other Parts Discussed in Thread: ADS1220
Hi,
Bellow experiment data was perfom in ADS1220 EVM board. The differential input was from AN1-AN2.
We had tested at different voltage reference,sps and pga gain,each test got form 512 samples and pick up
max/min value form 512 data. Customer need the pga gain bellow 8v/v because there sensor have bias voltage about 200mV
and this voltage is different from each sensor so they could not kill the bias voltage. The conversion speed need 600~1000 sps.
If the noise can reduce third or half they will choose ads1220 in there product. Could you give some advice to reduce the noise.
Whether ADS1220 can satisfied customer need.
Thnaks
| REF | SPS | GAIN | MAX | MIN | MAX-MIN |
| INT 2.048 | 660 | 1 | 92.52μVp-p | -85.69μVp-p | 178.22μVp-p |
| INT 2.048 | 330 | 1 | 63.96μVp-p | -63.23μVp-p | 127.19μVp-p |
| INT 2.048 | 330 | 4 | 57.12μVp-p | -67.62μVp-p | 124.75μVp-p |
| INT 2.048 | 330 | 8 | 52.00μVp-p | -75.68μVp-p | 127.68μVp-p |
| INT 2.048 | 175 | 8 | 41.50μVp-p | -50.53μVp-p | 92.0data.xlsx4μVp-p |
| EXT 3.3 | 660 | 1 | 74.74μVp-p | -98.34μVp-p | 173.09μVp-p |
| EXT3.3 | 330 | 1 | 53.89μVp-p | -57.43μVp-p | 111.32μVp-p |
| EXT3.3 | 330 | 4 | 44.45μVp-p | -74.35μVp-p | 118.80μVp-p |
| EXT3.3 | 330 | 8 | 51.53μVp-p | -70.81μVp-p | 122.34μVp-p |
| EXT3.3 | 175 | 8 | 42.87μVp-p | -48.38μVp-p | 91.26μVp-p |