Part Number: TSC2007
Hi team
I would like to inquire about TSC2007 function.
Touch Input is X +, X-, Y +, Y-.
Can I change this input to X-> X + with X + -> X- through register set?
If so, how do I set it up?
Thanks,
TM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSC2007
Hi team
I would like to inquire about TSC2007 function.
Touch Input is X +, X-, Y +, Y-.
Can I change this input to X-> X + with X + -> X- through register set?
If so, how do I set it up?
Thanks,
TM
Hello,
Unfortunately this is not possible. I've copied the block diagram (Figure 23) and register information (Table 3) below which shows that MUX settings for the X,Y,Z1, and Z2 measurement are set by default to the positions described. Is it possible to physically move the wires to match the X+ connections of the touch screen with the X+ input of the TSC2007?