Other Parts Discussed in Thread: LMK04828
Hi,
There are 3 available config files for the ADC3xJxxEVM using the HSDC Pro GUI - 80 MSPS, 128 MSPS, and 160 MSPS. I am using the ADC34J44EVM where the maximum clock frequency is 125 MHz. Is there any reason that a 125 MSPS config file is not available instead of the 128 MSPS?
If I use the 128 MSPS config file and set my sampling rate to 128M, is there anything I should be weary of given that it is greater than what has been rated as the maximum clock frequency?
Thanks,
CK