Hi support team,
Regarding power supply of DAC7716, is there a possibility of destruction of the IC when applying voltage as follows?
· AVDD - AGND : +15 V
· AVSS - AGND : -15 V
· DVDD-DGND : No supply (Normally added +5 V)
· IOVDD - DGND : No supply (Normally added +5 V)
· REF-A - REFGNDA : No supply (Normally added +3.3 V)
· REF-B - REFGNDB : No supply (Normally added +2.5 V)
* Voltage references (+3.3 V and +2.5 V) are generated from +5 V power supply
On the customer's board, when the power supply (+5 V) of DVDD and IOVDD was turned on and off several times while applying the power supply (±15 V) of AVDD-AGND and AVSS-AGND, the output voltage of only one channel shifted lower (about 0.4 V lower than the expected value).
What is the possible reason for the output voltage shift?
Sincerely,
M. Tachibana