I have a design which uses a DAC7563 to output a DC voltage used in a signal processing application. Noise on this voltage, especially around 2 MHz can effect our measurements.
There if a simple LC filter on the AVDD (3.3V) supply is adequate, or if we should add a separate low noise LDO to generate AVDD for this DAC.
What I would like to have is a graph of the power supply (AVDD) rejection ratio (PSRR) against frequency, which is common for op-amp datasheets.
My expectations is the PSRR should be good because of the VREF regulator. I have seen the VREF typical Line regulation at 25°C specification of 50 μV/V. Is this only for DC or is it valid at 2 MHz?
Thanks