Hi,
My ADS61B49 sometimes make output code of 0x3FFE (11111111111110) even if the input differential voltage is around 3V. Sometimes the same chip output code goes 0x3FFF.
I got such devices on my 2-3 boards (chips) out of 8 boards.
All those chips seems to be within the spec because the data sheet specifies input differential of -1dBFS. And the devices are not tested at over range inputs.
But for me this is curious because this doesn't happen for SAR ADC devices in my experience.
Are those devices, which make max code of 0x3FFE, not defective?
Kind Regards,