This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5812: Looking for an FPGA that interfaces with

Part Number: AFE5812


Hello, Currently i am looking to use the AFE5812 in a sonar application due to the many features that will help to complete my project however I am looking to see if there is an FPGA you would recommend that interfaces with this ADC as an FPGA will be much better for higher frequency application then a dsp. If you are able to also find a dsp that is able to handle this feat and can be compared to the FPGA that would also be an incredible help.

Thank you

Michael Ferreira