Other Parts Discussed in Thread: MSP430FR2633,
Hello All,
The Pin connection I did from below figure.
I'm using 10k resistor value as a pull-up and have a selected 100 kbps speed for I2C from the 8MHz SMCLK Clock.
I'm trying to interface ADS122C04 24-bit ADC with MSP430FR2633
I have written following algorithm:
1. Send Reset Command (0x06)
2. Write Configuration Register
a. Register 0 (0x40) = 0x81;
b. Register 1 (0x44) = 0x04;
c. Register 2 (0x48) = 0x00;
d. Register 3 (0x4C) = 0x00;
//Here I'm using Single short conversation mode and Single channel Read Mode
3. Send Start Command (0x08);
4.loop
{
Wait for DRDY Pin to transition low;
send Read Command (0x10);
}
The DRDY pin goes low after sending the start command.
The Above algorithm I have a implemented and I'm able to read only data = [0xFF, 0xFF, 0xFF] from ADC every time.
I'm also giving different voltage using potentio-meter on AIN0 Channel from 0 to 3.3v but I receive same data (data = [0xFF, 0xFF, 0xFF]) on different voltages.
Here is my 8MHz Clock Configuration:
{
__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source
CSCTL0 = 0; // clear DCO and MOD registers
CSCTL1 &= ~(DCORSEL_7); // Clear DCO frequency select bits first
CSCTL1 |= DCORSEL_3; // Set DCO = 8MHz
CSCTL2 = FLLD_0 + 243; // DCODIV = 8MHz
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
// default DCODIV as MCLK and SMCLK source
}
Here is my I2C Configuration:
{
UCB0CTLW0 |= UCSWRST; // Put eUSCI_B in reset state
UCB0CTLW0 |= UCMODE_3 | UCSSEL_3 | UCMST | UCSYNC; // I2C master mode, SMCLK
UCB0BRW = 0x33; // Set Bit rate 100 kHz
UCB0I2CSA = 0x40; // ADC122C04 slave Device address
UCB0CTLW0 &= ~UCSWRST; // Software Reset Disable
}
Please do needful.
Regards,
Kelvin