Other Parts Discussed in Thread: TIPD215
Hi,
I'm working on a project where I want to use the DAC8775 for two analog outputs controlled through SPI interface. I have used TIPD215 as a reference design but I have a few questions.
1. What should I do with the pins of unused channels ? ( Channels C and D)
2. Should I create two different grounds (for analog and digital) or is it not necessary?
3. What is the purpose of the switching diodes (BAV99) on the output of each channel?
4. If I'm not fitting the capacitor between CCOMP_x and output , should I leave the pin unconnected or connected to the output without capacitor?
I hope I have made no mistake in the schematic
Best regards,
Ondrej BrejlaProtAnalog2-ProtAnalog2.pdf