Hi Experts,
Can ADS1114IDGST coexist with standard PMBUS device on the same I2C interface? Any potential risk?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Can ADS1114IDGST coexist with standard PMBUS device on the same I2C interface? Any potential risk?
Thanks
Zhipei,
I've never run the ADS1114 with other PMBus devices on the same bus. However, PMBus is similar to I2C and much of the communication would be functional.
I did come across this post about I2C and PMBus:
e2e.ti.com/.../409022
It brings up some PMBus incompatibilities that might come up. On top of the points made in the post, I'd note that the SMBus has a maximum communication 100kHz. I would note that the ADS1114 is similar to SMBus in that there is a similar timeout and minimum bus speed required. Also, the I2C VHi and VLo levels are different between I2C and PMBus.
I did find an app note on implementing PMBus with the I2C hardware on the TMS320F2803x:
www.ti.com/.../sprabj6.pdf
Regardless, I don't know enough about PMBus implementation to know if there are more risks involved in running a PMBus device on the same I2C interface. I assume the previous app note covers this in more detail. It might help to post in the Power Management forum to see if they have any other information about this topic.
Joseph Wu