I install the ADS131 evb & install the driver, DELTASIGMAEVAL-GUI-installer
but system still can't find the evb as below,please advise it,thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I install the ADS131 evb & install the driver, DELTASIGMAEVAL-GUI-installer
but system still can't find the evb as below,please advise it,thanks
Alex,
For the ADS131A04EVM, there are two things that need to be installed. First, I think you have installed the Delta-sigma ADC EvaluaTIon software. However, you also need to install the ADS131A04EVM Evaluation Software Device Package. For each EVM that uses the EvaluaTIon software, there is a separate device package written for each EVM.
Unplug the EVM, and install the ADS131A04EVM Evaluation Software Device Package. This can be found on the ADS131A04EVM landing page. In the "Order Now" section, you should be able to find the Download button for the device package.
If there are some driver problems, you may need to do some debugging. There are some basic recommendations in section 2.3.2 in the Delta-Sigma ADC EvaluaTIon Software User Manual.
After installation, post back here. If this solves the problem, great. If this doesn't fix the problem, we can look at other solutions.
Joseph Wu