This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D1000RF: Device ADC12D1000RFIUT/NOPB need US re-export license required?

Part Number: ADC12D1000RF

MPN: ADC12D1000RFIUT/NOPB  ECCN is 3A001.a.5.a.3,

I need to get manufacturer/supplier written/email confirmation on the part if it is

1) "designed or modified" for military use,

2) Hermetically sealed and

3) Rated for operation in the temperature range from below -54 Degree Celsius to above +125 Degree Celsius

 

Now customer will be Development & Manufacturing of Industrial tester, power supply.

1. Product Usage - Narin is end user using this part for Ground Noise Monitoring module development.
2. Product Functionality - High speed Analog to Digital converting for Arch Noise (Impulse) Detecting & Monitoring from ground.
3. Product Application - This is installed on a High-Power Transmit Cable buried underground and periodically checks the impulse noise (Arch Noise) of the joint surface. also store and analyze/manage data for at least three months. Impulse Noise is instantly communicated to the user and the power is shut off until appropriate action is taken. This is a monitoring device for high-power transmission lines.