Hi TI expert,
I wonder if DAC900's VA(analog supply) and VD(digital supply) can both be +3.3V? I have this question because DAC900's datasheet says that its VA and VDs' typical values are both +5V.
Besides, can DAC900's pin 25 be connected to digital ground?
I have such two qustions just because that I want to build a PCB having the TSSOP-28 footprint suitable for TI's DAC900 and ADI's AD9740. I have a third question, is this ok, if I feed DAC900 with clock rate of 150MHz and AD9740 with 200MHz. AD9740's link is given here, https://www.analog.com/media/en/technical-documentation/data-sheets/AD9740.pdf
Regards
Yatao