Other Parts Discussed in Thread: ADS122C04
We have installed Delta-Sigma ADC Evaluation Software and the Device package for ADS122C04 (ADS122C04-dvcpkg). These were installed using Administrator privileges on Windows 10. The software is not able to connect with the EVM. Two potential issues that we see are:
1. Windows Device Manager indicates there are no associated drivers for the EVM. Here's an image showing the Device Manager entry for the EVM.
2. What is the purpose of the switch S2 on the EVM? Does closing this switch cause an issue with the EVM?
Please note that we do not see any method of selecting the EVM when the software is started. This is what appears:
The text in the lower left changes to "Hardware Not Connected. Ready..." after several seconds.
The EVM is attached to the computer via a USB port located on the motherboard using the supplied USB cable.
- John