We are planning to use the TSW1400EVM card to capture the ADC outputs from an ADS4246EVM ADC evaluation board.
Do I understand correctly that the HSDC Pro v5.00 software controls both the capture card and the ADC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are planning to use the TSW1400EVM card to capture the ADC outputs from an ADS4246EVM ADC evaluation board.
Do I understand correctly that the HSDC Pro v5.00 software controls both the capture card and the ADC?
Also, added question:-
Another question please. We will need to run multiple tests with the eval board and it would be very helpful to automate them. Is there any kind of api that we could use to control the eval software? The minimum we need to do is to set the destination for the capture file and then start and stop a continuous capture. Our preferred software for the automation is Python.
Hi Ajayt,
Yes, this should not be an issue. The HSDC Pro software is setup for automation, and can be controlled using MATLAB, LabVIEW and Python, and there are examples to get you started. Please see the HSDC Pro folder "C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro 5.0\HSDCPro Automation DLL\Manual and Examples" for automation documentation and examples.
Best Regards,
Dan