This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC0808-N: Power Sequence for VCC and VREF?

Part Number: ADC0808-N
Other Parts Discussed in Thread: TLV4170

I am troubleshooting an issue on a design that uses an ADC0808-N.  One observation I have made is that I get different behavior depending on whether I apply voltage to the VCC pin before VREF, or vice versa.

SETUP:

The VCC pin is receiving power from a +5 V supply and is connected directly to the power rail.

The VREF+ pin is connected to +5 V derived from a separate power supply than the VCC +5 V rail.  The derived +5 V goes through an op-amp voltage follower (TLV4170) who's output is then connected to VREF+.

The VREF- pin is connected to ground.

TEST:

When I am powering up the ADC, if I apply voltage to VCC first, and then to VREF+, the ADC works as expected.

However, if I apply voltage to VREF+ first, and then to VCC, I notice that the VREF+ plus pin has dropped from +5 V to about +4.6 V.  The output of the voltage follower has dropped to +4.6 V even though its input is still at +5.0 V.  It seems like the ADC is in some state where the VREF+ pin is loading down the op-amp.

Anyone know anything about this behavior?  Any ideas would be appreciated!