Other Parts Discussed in Thread: ADC12DL3200EVM, ADC12DL3200,
Hi, There was a discussion between TI customer and support regarding "... ADC12DL3200EVM, TSW14DL3200EVM, #adc12dl3200, #Firmware, # Development, #ADC, #FPGA..." ending on Jul 19, 2018 7:50 PM In reply to adeel asif by TI support member Jim s.
My question is similar in nature and would like to see if the solution was made available as stated and would like to get it. The response, on Jul 19, 2018" from Jim ended as follows:
"Adeel,
This firmware will not be available for at least another 30 days.
Regards,
Jim s"
Is it available now and can we get it. To make it more clearer, if there is a simpler solution, what we needed is to use some form of programmatic control to collect|send data from the ADC capture board. A DotNET dll or some API would do just fine if we can get it, not necessarily the FPGA code... An example would be ADIs AD9295 Visual Analog that does have a GUI control just like the HSDC Data Converter Pro GUI but also has DotNET dlls available to create wrappers and get data from the capture board from test programs like LabVIEW.
We are ready to order the 1st kit pending a response for it. Please get back to us asap.
Regards,
Mesfin Teshome
Teledyne Scientific & Imaging, LLC
1049 Camino Dos Rios
Thousand Oaks, CA 91360
www.teledyne-si.com
Office:805-373-4078, Fax:805-373-4860