Other Parts Discussed in Thread: TIDA-00996,
Dear all,
is there anyway to generate 4 independent outputs from the DAC38J84 ?
For instance, what about bypassing the NCO ?
regards,
Domenico
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
is there anyway to generate 4 independent outputs from the DAC38J84 ?
For instance, what about bypassing the NCO ?
regards,
Domenico
Hi Kang,
thanks, but the concerns is more related to the capability of the memory to send data.
In the feature of the TSW14J56EVM I can read "Quarter rate DDR3 controllers supporting up to 800MHz DDR3 operation".
Since I'm not familiar with the terms "Quarter rate", can the memory tranfer the data to the DAC in order to have a fs=960MHz for each channel ?
If it is not possible, can the TSW14J57 do the job with DAC38j84EVM ?
regards,
Domenico
Domenyko,
The HSDC PRO load the playback pattern into the TSW14J56 memory (or DDR) and the pattern gets played back repeatedly.
All the clocking and the gear box ratio are handled within the firmware so you do not need to be concerned about the implementation. You can be assured that the pattern inside the DDR gets played back at 960MSPS.
-Kang