Other Parts Discussed in Thread: THS4521, ADS8353
Hello,
I was wondering how to terminate the the negative input when using single-ended input signal?
Thanks & regards,
-albin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Albin,
The ADS8354 requires a fully differential configuration. You cannot connect either input to ground and meet the datasheet specifications.
The Vcm specification in the datasheet only allows Vref+/-0.1V or Vref/2+/-0.1V depending on the input range selected.
In order to drive the inputs differentially, you can use the THS4521 fully differential amplifier (Figure 100 in the datasheet), which can be configured as a single-ended input. Take a look at the following two 'Circuit's' that show how to do this.
http://www.ti.com/lit/an/sbaa264/sbaa264.pdf
http://www.ti.com/lit/an/sbaa246/sbaa246.pdf
Regards,
Keith N.
Precision ADC Applications