Dear Sir,
A customer would like to tie AVSS-SW to ground and switch REFN0 for external application to connect ground or float. I read section 10.1.5 on page 89 in d/s as follows;
"REFN0 is an exception; this pin can be accidently shorted to AVSS through the internal low-side switch. Leave the REFN0 pin floating when not in use or tie the pin to AVSS."
It looks keeping REFN0 floated is okay, but I wonder if it is better to have a capacitor between REFN0 and ground to avoid (AVSS-SW switch) noise?
Best regards,
Masa