Dear Sir,
May I ask if Filter Response will mainly get impact from internal oscillator temperate deviation?
I am estimating filter response using ADS1x4S0x Caluculator.xls.
My idea is;
I get Filter frequency response of Low-Latency Filter with 16.6SPS for example:
I understand that 50Hz notch is centered when fCLK=4.0960MHz.
I am keen to the internal oscillator will move the filter response, then
I refer to the following internal oscillator spec
and read min and max values of 28 samples in Figure 25.
then below is summary;
The accuracy of +/-1.5% will rigidly cover across PVT.
Now I get filter response by changing max deviation of fCLK to 4.157MHz as follows;
It is till -29.09dB attenuation for 50Hz line cycle.
If there is another factor to consider which will impact the filter frequency response, please let me know.
Best regards,
Masa