Other Parts Discussed in Thread: TIDA-01021, LMK04828, LMX2594, ADC12DJ3200, TSW14J57EVM
Hello,
I'm trying to synchronize two ADC12DJ3200EVM boards using a TIDA-0121 board. I need the boards to be configured as follows:
1) TIDA-1021 External Oscillator Reference of 10MHz or 100MHz instead of the on-board references.
2) ADC12DJ3200EVM in JMODE0 @4GSPS
3) TIDA-01021 DCLK out at 2GHz.
Is it possible to operate the in the configuration described above? If so, could you provide the changes I would need to make to the configuration files that come with the software?
Thank you,
Apurva