Part Number: ADC12J1600EVM
Hello,
I am starting to use the ADC12J1600 together with the TSW14J56.
Following the specification file slau56.pdf. I installed both the ADC12J1600EVM GUI and the High Speed Data Converter Software. The TSW14J56 connects properly to the computer. However when I open the GUI for the ADC, I get the error "FT_DEVICE_NOT_FOUND''. As suggested I downloaded the FT_PROG software and I get as in the picture below. Which seems to imply that the ADC is ok.
There are a couple of things that I do not quite understand and that might be related.
1) In the High Speed Data Converter when I try to select the ADC, I do not see any ADC12J1600 but just the ADC12J4000
2) There are two red leds at the centre of the ADC12J1600EVM, which I am not sure should be there.
Is there anything I should try to make this work properly?
If anyone as any idea of how to sort this, it would be very useful.
Kind Regards,
Francesco