Part Number: ADS1013
Other Parts Discussed in Thread: ADS1018
Hi Team,
I want to use the largest pull up resister(Like 100k ohm) for ADS1013 I2C communication to reduce total current consumption of a system.
But Max tR is specified as 300ns at 7.6 Timing Requirements: I2C in the datasheet. Slower communication rate like 10kHz is acceptable for system requirement but it will be hard to keep the tR and tF requirement if i choose 100k ohm as pull up resister in the system.
Then I have following questions.
1. Is it possible to use slower tR rate with low speed communication such as 10kHz clock rate?
(In other word, can we use 100k ohm as pull up resister in the system using ADS1013?)
2. If the answer for question above is NO, Why the value is limited to 300ns?
Regards,
Takashi Onawa