Hi,
According to datasheet of ADS124S06 (page 6) we need to connect a 1-μF to 47-μF capacitor to REFCOM if the internal voltage reference is enabled.
My problem is that if this capacitor is placed, the consuption current increse about 25mA. I checked the hardware and firmware but i haven't found the problem yet.
Without the capacitor it works well.
Any suggestions to try to solve the problem or can I leave like this without the capacitor?
Thanks
Edson