I have a question regarding the possible current source options that exist for doing AC lead-off measurements on the ADS1296R.
pg. 40 of the ADS1296R datasheet says "AC Lead-Off: The AC signal is generated by providing pullup and pulldown resistors at the input with a fixed frequency." This makes it seem like pull-up/pull-down resistors are the only possible way to generate AC current. When we look at the register 4 bit options, however, it seems like there is also a current source option for doing AC lead-off.
My questions are:
1. Can register 4 be set to a value of 0x0d? i.e. a 24nA (48nAp-p) AC lead-off measurement using a current source.
2. Can you clarify the options?
For AC lead-off: register 4 bit 4 must always be 1 (pull-up resistor mode)? Or can it also be 0 (current source mode)?
For DC lead-off: register 4 bit 4 can be either 0 (current source) or 1 (pull-up resistor). Is that correct?
Thanks so much for your help