This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC112: Isolation resistor

Part Number: DDC112


I am designing an instrument based on the DDC112 as a student project.

The lower part of figure 29 in the datasheet shows the DVDD power supply derived from the AVDD supply with a < 10 ohm isolation resistor. I would be grateful if someone could explain how the resistor protects the analog supply from noise. The isolation resistor is absent in Application Note MULTI-DDC112 BOARD DESIGN (figure 1a) as well as in User Guide DEM-DDC112U-C EVALUATION FIXTURE (figure 10). 

I also noticed that the Application Note MULTI... (figure 1a) has decoupling capacitors of 1uF at the supply inputs and the User Guide DEM-DDC.. (figure 10) has 10uF + 0.1uF. Why so?

Regards,

Christer